Depending on your needs, you can install all EcoStruxure Building Operation products or a few products, such a single SmartX server with a connected WorkStation.
WorkStation is the interface where you supervise your EcoStruxure BMS. In WorkStation you can also create, modify, and delete some of the objects that are used to build an EcoStruxure BMS.
Ensure that you have a working and available WorkStation license. A working license is required to log on to WorkStation. Pour plus d'informations, voir Licenses .
When you install WorkStation, you have the option to install the bundled tools: Graphics Editor, Script Editor, Menta Editor, Function Block Editor, and WorkPlace Tech. WorkStation is required to run these client tools.
Pour plus d'informations, voir WorkStation .
You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.
You have to have a valid Graphics Editor license to start the Graphics Editor. Pour plus d'informations, voir Licenses .
The installation of Graphics Editor is bundled into the WorkStation installation package.
Pour plus d'informations, voir Graphics Editor .
Script Editor is a text programming tool you use to create Script programs that control and monitor building automation systems. For example, in WorkStation, you can create a basic program, called OfficeLights, to control lighting and ventilation in a room based on occupancy.
Ensure that you have a working and available Script license. A working license is required to start Script. Pour plus d'informations, voir Licenses .
The installation of Script Editor is bundled into the WorkStation installation package.
Pour plus d'informations, voir Script Editor Program Creation .
Menta Editor is a graphical programming tool for Xenta 208/300/401 LonWorks device, which you use to create function block programs that control and monitor building automation systems. For example, you create a program to control an air handling unit.
Ensure that you have a working and available Menta Editor license. A working license is required to start the Menta Editor software. Pour plus d'informations, voir Licenses .
The installation of Menta Editor is bundled into the WorkStation installation package.
Pour plus d'informations, voir TAC Menta ., Technical Manual (04-00030).
Function Block Editor is a graphical programming tool for EcoStruxure BMS servers and MP Series controllers, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.
Ensure that you have a working and available Function Block Editor license. A working license is required to start the Function Block Editor software. Pour plus d'informations, voir Licenses .
The installation of Function Block Editor is bundled into the WorkStation installation package.
Pour plus d'informations, voir Function Block Editor Overview .
The WorkPlace Tech component of WorkStation consists of two graphical tools: WorkPlace Tech Monitor and WorkPlace Tech Editor. With WorkPlace Tech Editor, you can create, modify, monitor, and troubleshoot MNL LonWorks and MNB BACnet device applications. With WorkPlace Tech Monitor, you can monitor and troubleshoot applications in MNL LonWorks and MNB BACnet devices.
Ensure that you have a working and available WorkPlace Tech license. A working license is required to start the WorkPlace Tech Editor or WorkPlace Tech Monitor software. Pour plus d'informations, voir Licenses .
The installation of WorkPlace Tech is bundled into the WorkStation installation package, and is specific to the particular version of WorkStation in that package.
The WorkPlace Tech Editor component requires the installation of the appropriate version of Microsoft Visio.
Pour plus d'informations, voir WorkPlace Tech Editor .
Pour plus d'informations, voir Information Technology System Planning Guide .
Pour plus d'informations, voir WorkPlace Tech Overview .
Enterprise Central is the hierarchical EcoStruxure BMS server at the top of the system architecture hierarchy of a large Building Management System. Enterprise Central is primarily used for administration and data aggregation in an EcoStruxure BMS that has multiple Enterprise Servers. From one location, you can manage operations across large Building Management Systems that have multiple Enterprise Server subsystems.
Pour plus d'informations, voir Enterprise Central .
Enterprise Server is the hierarchical EcoStruxure BMS server at the top of the system architecture hierarchy of a medium size Building Management System, or at the middle of the hierarchy in a large system. Enterprise Server is primary used for administration, system supervision and engineering of SmartX servers. Enterprise Server aggregates data that can be accessed by Enterprise Central.
Ensure that you have a working and available Enterprise Server license. A working license is required to start the Enterprise Server. Pour plus d'informations, voir Licenses .
Pour plus d'informations, voir Enterprise Server .
The Software Administrator installs with the Enterprise Server installation package. You use the Software Administrator to start and stop the Enterprise Server service and configure the ports of the Enterprise Server.
Pour plus d'informations, voir Software Administrator .
The Device Administrator is used to configure and upgrade the software of EcoStruxure BMS servers through a network or USB connection.
The License Administrator administers the activation, return, and repair of licenses.
Pour plus d'informations, voir License Administrator .
The License Server manages the administration of network licenses. An EcoStruxure BMS running with network licenses must contain at least one License Server.
Pour plus d'informations, voir License Server .
The License Server Installation is bundled into the License Administration installation package.
WebReports is a Web application that you use to create, view, and administer reports. The reports provide information about alarms, trends, and user and system activity. You use the reports to help manage your building automation system.
Pour plus d'informations, voir WebReports Overview .
At the main installation, WorkStation contains English and languages that are avaílable at the time. To support a language, WorkStation needs the specific language package.
Pour plus d'informations, voir Language Packages .