earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/2/2024

Progress View – Simple

The Progress view displays information about time-consuming operations between WorkStation and the EcoStruxure BMS server. You can also see detailed information about what went wrong if the operation fails. The Simple Progress View is displayed when you create, rename, copy or move, an object. If the operation is successful and very fast you may probably not notice the Progress view at all.

 
action_zoom_plus_stroke Simple Progress view when an operation failed.
Figure: Simple Progress view when an operation failed.
  • Progress View – Advanced
  • Progress View
  • Error Details – Progress View
  • Operation Details Dialog Box