earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Automation Server, AS-B, Enterprise Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.9
12/14/2016

Quick Filter

You use Quick filter to filter out the objects by their names from the list. You can either type the name in the Quick filter box or drag an item from a column in the Alarms pane, the Events pane, an Alarm view, or an Event view and drop it in the Quick filter box.

For example, if you want to find all objects that are named “temperature”, just type “temp” in the Quick filter box and only objects named temperature are displayed in the list. 

 
action_zoom_plus_stroke Filtering on characters in all visible columns
Figure: Filtering on characters in all visible columns

The Quick filter filters on everything that is visible in the columns in the List View. For example, if you filter on “2” you do not get any hits. But if you add the columns Note 1 and value you get hits on the temperature, which is 21, the setpoint which is 20, and the Note that the program controlling the fan is a model 22.   

 
action_zoom_plus_stroke Quick filter filters on all visible columns in the view
Figure: Quick filter filters on all visible columns in the view

​Quick filter is used in the following components in WorkStation:

  • ​List View

  • Alarms pane

  • Alarm Views

  • Events pane

  • Event Views

  • Alarm or Event details views

  • Watch pane

  • Watch Views

  • Add/Remove columns dialog box

  • Create object wizard

 
action_zoom_plus_stroke The Quick filter is used in many components, such as the List View (upper right), the Watch pane (bottom left), and the Add/Remove dialog box (center right).
Figure: The Quick filter is used in many components, such as the List View (upper right), the Watch pane (bottom left), and the Add/Remove dialog box (center right).
  • Basic Functions
  • Alarms Pane and Alarm View
  • Alarm and Event Detail View
  • Watch Pane and Watch View
  • Add/Remove Columns Dialog Box (List View)