You use a structured database editor to view archive information in rows and columns, which may contain text strings, paths, identities, or enumeration values.
The time stamps for each record in the archive file reflect the UTC rather than local machine time.
The following table provides an overview of an archive file. The number and type of columns that display varies with the log that is viewed. For example, trend logs have a different set of column headers than event logs due to the data content.
Column |
Description |
AcknowledgeTime |
Displays the time and date when the alarm was acknowledged. |
AlarmState |
Displays the present alarm state. |
AlarmText |
Displays the alarm message that was added to the alarm. |
AssignedState |
Displays the assigned state the alarm had. |
AssignedToDomain |
Displays the domain to which the user or group was assigned. |
AssignedToName |
Displays the name of the user or group to which an alarm was assigned. |
AssignedToUniqueUserId |
Displays the unique ID of the user or group to which an alarm was assigned. |
BACnetEventType |
Displays the BACnet event that occurred within a BACnet network. |
BasicEvaluationState |
Displays the basic evaluation state of an alarm. |
Category |
Displays the name of a category. |
Command |
Displays the executed command. |
Comment |
Displays the comment that was added to an alarm. |
ControlDescr |
Displays the descriptive information about the I/NET operator. |
ControlSource |
Displays the initials of the controlling I/NET operator. |
Count |
Displays the number of times the alarm has toggled between the alarm and reset state. |
CWSId |
Displays the ID of the EcoStruxure Web Service (EWS) object. |
CWSSourceId |
Displays the ID of the EWS source object. |
CWSSourceName |
Displays the name and path of the EWS source object. |
Description |
Displays a brief summary of the major features or characteristics. |
DeviceName |
Displays the name of an I/NET device that generated the event. |
DisabledCause |
Displays the reason why the alarm was disabled, such as a shunt variable. |
DomainName |
Displays the domain to which a user belongs. |
EndTime |
Displays the time when the old meter was replaced. |
EndValue |
Displays the value the old meter had when it was replaced. |
EvaluationState |
Displays the present evaluation state of the alarm, such as Upper limit alarm. |
Event |
Displays an event that occurred within the network. |
EventGUID |
Displays the unique identity of the event. |
FirstName |
Displays the first name of the individual whose key/card was used at the I/NET door point. |
ForcedValue |
Displays the forced value events. |
GroupName |
Displays the name of the cause note or action note group the user edited. |
Hidden |
Displays the visible status of an object, such as False. |
InetAddr |
Displays the system address of the point, or station address of the host or controller that generated the event. |
IndivNdx |
Displays the number of the individual whose key/card was used at the I/NET door point. |
InetEventTypeId |
Displays the IDs of the I/NET event types generated by the system. |
ItemName |
Displays the name of the check list, cause note, or action note group the user edited. |
LastName |
Displays the last name of the individual whose key/card was used at the I/NET door point. |
LinkName |
Displays the name assigned to the link of the device from which the event originated. |
LogType |
Displays the type of the trend log that has been edited. |
MaxValue |
Displays the last value of the new meter before roll-over. |
MessageText |
Displays the text of an I/NET action or dispatch message. (Optional) |
MeterConstant |
Displays the constant of the meter in a meter trend log. |
MinValue |
Displays the first value of the new meter after roll-over. |
MonitoredValue |
Displays the path of the monitored variable. |
MonitoredValueType |
Displays the type of monitored value that triggers an alarm, such as Forced. |
MonitoredVariable |
Displays the path of the monitored variable. |
Note |
Displays the text entered into the Note 1 property. |
OriginalSeqNo |
Displays the RefSeqNo collected from a trend log. This number is only written on an extended trend log containing records that were changed on the connected trend log. |
OriginatedGUID |
Displays the unique identity of the source. |
PreviousAlarmState |
Displays the previous alarm state. |
Priority |
Displays the current priority of the alarm. |
RefSeqNo |
Displays the unique sequence number of a record that has been edited. |
SEQNO |
Displays the sequence number of the record. |
ServerOffline |
Displays the online/offline status of an EcoStruxure BMS server. |
Source |
Displays the name and path of the source object. |
SourceServer |
Displays the name and path of the source object. |
StationName |
Displays the name assigned to the controller from which the event originated. |
StartTime |
Displays the time when the new meter was installed. |
StartValue |
Displays the value of the new meter when it was installed. |
Status |
Displays the status of the trend log. |
SystemAlarmId |
Displays the alarm ID generated by the system. |
SystemEventId |
Displays the event ID generated by the system. |
TenantNdx |
Displays the tenant number of the individual whose key/card was used at the I/NET door point. |
TextField |
Displays the information entered into the Text property. |
TimeStamp |
Displays the date and time when the record was generated. |
TriggeredTimestamp |
Displays the time and date an alarm went from normal state to alarm state. |
TYPE |
Displays the object type that defines the properties of the object. |
UniqueAlarmId |
Displays the unique alarm ID of an alarm. |
UniqueUserId |
Displays the unique identity number of a user. |
Unit |
Displays the selected unit of a value, such as °F (Fahrenheit). |
User |
Displays the user who generated the event. |
UserName |
Displays the name of the user who generated the event. |
Value |
Displays the value of a record. |
ValueAfter |
Displays the value of an object after it was changed. |
ValueBefore |
Displays the value of an object before it was changed. |
Zone |
Displays the I/NET security zone number associated with a security event. |
An enumeration is a range of values representing a specific command or event.
有关更多信息,请参阅 Event and Alarm Enumerations .
An enumeration is a range of values representing a specific command or event. Trend log properties use two enumeration values: Events and Status.
有关更多信息,请参阅 Trend Log Enumerations .