By default, WorkStation presents language, date, time, currency, unit, and decimals according to the regional settings of the user’s operating system.
The date, time, or value format can differ between clients that have the same language and cultural convention.
For example, a user customizes the French date setting to yyyy-mm-dd in the operating system. The next time WorkStation starts on this client, all dates are displayed as yyyy-mm-dd instead of the French standard dd/mm/yyyy. Other clients with French original settings still display dates with the French standard dd/mm/yyyy.
The EcoStruxure Building Operation software supports several different languages. To be able to install a new language you need a language pack.
有关更多信息,请参阅 Language Packages .
The EcoStruxure Building Operation software handles values and numbers with the highest precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.
有关更多信息,请参阅 Value Presentation .
A time zone is a region on the earth that has a uniform standard time, usually referred to as the local time. Local time is the UTC time plus the current time zone offset for the considered location. Some time zones also have an offset called DST added during the summer period. The DST offset is typically +1 hour.
有关更多信息,请参阅 Time and Time Zone .