earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AD v1
Functionalities: Hardware
Product version: 3.3, 2022, 2023, 2024
7/23/2021

Installing the AD v1 Base on a Cabinet

You install the AD v1 protective frame with its base on a control cabinet to use AD v1 for locally accessing the automation servers. You attach the base on the cabinet using the dedicated holes in the base.

Note:

The frame and its base do not provide protection against theft.

Show More
action_close

AD v1 provides a Human Machine Interface (HMI) for local access to the EcoStruxure BMS servers.

AD v1 is based on an Android platform with a high-resolution touchscreen display. The display size is 10 inches.

 
action_zoom_plus_stroke AD v1
Figure: AD v1

Stationary HMI Terminal

AD v1 is intended to be used as a stationary HMI terminal. For example, AD v1 can be installed on a control cabinet in a plant room or it can be installed on a wall in a hospital.

Kiosk Mode

AD v1 is preinstalled with SmartXKiosk, which allows you to lock AD v1 into Kiosk mode to prevent users from accessing other apps than the one you have downloaded and selected. For more information, see SmartXKiosk Overview .

AD v1 Bundle

AD v1 is delivered in a bundle, which contains a protective frame. When assembled, the frame protects against dust, moisture, and mechanical damage. The USB cable is ordered separately from Schneider Electric.

Note:

The frame and its base do not provide protection against theft.

Installation Options

The protective frame has a base, which is equipped with hole mount patterns to support a variety of installation options. For example, AD v1 can be installed on a control cabinet, on a wall, or on a VESA stand that fits devices with a 100 x 100 mm (3.94 x 3.94 in.) hole pattern.

AD v1 Communication and Power

AD v1 can use either a wired (USB) connection or a wireless (WiFi) connection to communicate with EcoStruxure BMS servers. AD v1 can be powered either by a AS-P server, AS-B server, or USB power adapter.

For more information, see AD v1 Communication and Power .

Preinstalled Apps

AD v1 is delivered with the following set of preinstalled apps:

  • SmartXKiosk for locking AD v1 into Kiosk mode

  • AD-Link for enabling IP over USB communication

    For more information, see AD-Link Overview .

  • Technician Tool for operation and maintenance of EcoStruxure BMS servers

Specifications

Electrical
DC input current consumption
500 mA to 1.3 A
DC input supply voltage
5 VDC (USB)
Environment
Ambient temperature, operating
5 to 35 °C (41 to 95 °F)
Material
Enclosure
UV stable ABS
Ingress protection rating
IP 54
Plastic flame rating
UL94 HB
Mechanical
Dimensions (W x H x D)
266 x 203 x 19 mm (10.5 x 8.0 x 0.75 in.)
 
action_zoom_plus_stroke
Weight
0.656 kg (1.446 lb)
Communications
USB
1 USB 2.0 port
WiFi
802.11 a/b/g/n 2.4 + 5 GHz
CPU
Frequency
1.2 GHz
Type
Quad-core
Internal memory
1.5 GB RAM, 16 GB ROM
Operating system
Supported versions
Android 4.4 to 4.4.4 (KitKat)
  
Android 4.4W to 4.4W.2 (KitKat)
  
Android 5.0 to 5.1 (Lollipop)
Display
Display resolution
1280 x 800 pixels
Display size
10.1 inches (256 mm)
Display type
TFT LCD, touchscreen

To install the AD v1 base on a cabinet
  1. Hold the base in place against the cabinet.

  2. Mark the place where the center hole (cable insertion hole) should be on the cabinet.

  3. Remove the base.

  4. Create a 22 mm (0.87 in.) diameter hole in the cabinet.

    Tip:

    Use a metal hole punch to create the hole in the cabinet.

  5. Fit the cable grommet into the center hole in the base.

  6. Turn the cable grommet counterclockwise until it snaps into place in the base.

  7. Put the base on the cabinet with the cable grommet inserted through the center hole in the cabinet.

  8. Thread the nut onto the cable grommet.

  9. Level the base.

  10. Mark the place where the four drill holes (for attachment of the base) should be on the cabinet.

    Note:

    Use the holes in the corners of the base to mark the place where the drill holes should be.

  11. Remove the nut.

  12. Remove the base.

  13. Drill four holes in the cabinet.

  14. Put the base on the cabinet and fasten the base using four screws.

  15. Thread the nut onto the cable grommet and then tighten the nut.

     
    action_zoom_plus_stroke

You can now continue by installing the tablet in the frame.

  • AD v1
  • Installing the AD v1 Base on a Wall
  • Installing the AD v1 Tablet and Frame