When you log on to an Enterprise Server, you can perform remote backups of any SmartX server in the system. Whenever a backup occurs on the SmartX server, the system overwrites the locally stored file on the SmartX server with the new backup file. The Enterprise Server then retrieves and stores this backup file in a separate directory on the computer that runs the Enterprise Server.
When you want to restore a SmartX server, the system displays only the valid SmartX server backup files that are stored on the Enterprise Server.
In the event that the backup file on the SmartX server is damaged or lost, or not the one you want to use, you can select a valid backup file to restore the SmartX server. The restore operation overwrites the locally stored SmartX server backup file located on the SmartX server with the selected backup file. For more information, see Restoring a SmartX Server from the Enterprise Server .