Productos AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 2.0, 2.1, 3.0, 3.1
13/12/2018

Removing a Lead Rule from a Backup Rule

You remove the lead and shadow relationship from an EcoStruxure BMS server by deleting the lead rule reference.

Mostrar más
action_close

The EcoStruxure Building Operation scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on an EcoStruxure BMS server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

The EcoStruxure Building Operation software automatically backs up all data on an EcoStruxure BMS server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different EcoStruxure BMS servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one EcoStruxure BMS server, which acts as the lead, to manage a recurring backup for a group of EcoStruxure BMS servers. Para obtener más información, consulte Backup Rules View .

To remove a lead rule from a backup rule
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. In the Backup and Archiving area, click Backup rules .

  4. In the Backup rules view, select the backup rule and click the Edit backup rule button

     
    action_zoom_plus_stroke
    .

  5. In the Backup Rule dialog box, in the Lead rule box, delete the lead backup rule, which removes the lead and shadow relationship for the selected EcoStruxure BMS server.

  6. Click OK .

  7. On the File menu, click Save .

  • Backup Rules
  • Scheduled Backups
  • Editing a Backup Schedule
  • Backup Rules View
  • Backup Rule Dialog Box