earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Modalità

Modalità


Prodotti: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 1.8
13/10/2016

Removing a Lead Rule from a Backup Rule

You remove the lead and shadow relationship from a SmartStruxure server by deleting the lead rule reference.

Mostra di più
action_close

In Building Operation, scheduled backups are managed by backup rules, which are conditions that govern behavior. Similar to a scheduled task, a backup rule performs a backup on a SmartStruxure server using three pieces of data: when the backup occurs, what type of data will be backed up, and a comment describing the purpose of the backup.

Building Operation automatically backs up all data on a SmartStruxure server every Sunday at 01:00. However, you can change the backup rule settings. For example, you can change the type of data you want to back up.

You can create your own backup rules to complete different tasks on different SmartStruxure servers. For example, you can create a backup rule that backs up all data on the Enterprise Server twice a day rather than once a week based on the default setting. In addition, you can set up another backup rule for one SmartStruxure server, which acts as the lead, to manage a recurring backup for a group of SmartStruxure servers. Per maggior informazioni, consulta Backup Rules View .

To remove a lead rule from a backup rule
  1. In WorkStation, on the Tools menu, select Control Panel .

  2. In the Servers box, select the SmartStruxure server where you want to remove a lead rule from a backup rule.

  3. In the Backup and archiving area, click Backup Rules .

  4. Select the backup rule and click the Edit backup rule button

     
    action_zoom_plus_stroke
    .

     
    action_zoom_plus_stroke
  5. In the Lead rule box, delete the lead backup rule, which removes the lead and shadow relationship for the selected SmartStruxure server.

     
    action_zoom_plus_stroke
  6. Click OK .

  7. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Backup Rules
  • Scheduled Backups
  • Editing a Backup Schedule
  • Backup Rules View