Productos License Administrator, License Server
Funcionalidades: Gestión de licencias
Versión del producto: 2.0, 2.1, 3.0, 3.1
06/11/2018

Removing a Local License or Returning a Network License

You remove local licenses or return network licenses to the License Activation Server. For example, you can clean up expired licenses from the Licenses view or move network licenses to another License Server.

Aviso

You cannot reactivate a removed local license.

  • When you return a license to the License Activation Server, all the licenses that were activated in the same transaction with that license are also returned.

To remove a local license or return a network license
  1. In License Administrator, click the Licenses view.

  2. Select the local license to remove or the network license to return.

  3. On the Licenses toolbar, click the Remove/return license button

     
    action_zoom_plus_stroke
    .

  4. Click Yes .

  5. Click Close .

  6. In the Licenses dialog box, click Restart now , to apply the changes to the License Server.

  • Activating Network Licenses
  • Activating a Local License
  • License Maintenance
  • Local License Management
  • Licenses View Icons
  • Unable to Activate or Return a License
  • Licenses View