earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
功能: 基本功能
产品版本: 1.8
2016/10/13

Renaming a Folder or Object

You rename a folder or object to make the name more suitable to your needs.

注释:

When changing the name of a folder or SmartStruxure server, you also have to reconfigure users and user groups path permissions to this SmartStruxure server or folder. 有关更多信息,请参阅 Path Permissions .

注释:

You cannot change the name of a domain that is shared between SmartStruxure servers.

显示更多
action_close

You can move, copy, paste, rename, and delete objects from the Building Operation database at any time. To help you identify the object references that are affected when you delete an object, Building Operation displays a dialog box with information about references.

Move

Move does not affect the references. When you move an object, that object still references the same objects it referenced before you moved it. Objects referring to a moved object still refer to the same object after the move. Object cannot be moved between SmartStruxure servers however.

Paste

Paste removes all external references that are relative  but keeps absolute and locked references. 

Paste Special

Paste Special does the same thing as Paste but with the added benefit of keeping all of the external references.

Rename

Objects that are referring to each other do not lose their references if you change the name of an object. Building Operation automatically updates any references after you have renamed an object.

Delete

When deleting an object, you can select to keep the reference in other objects to the object you want to delete. You can then add a new object with the same name on the same location and all references are valid. This can be used if you, for example want to replace an analog value with a digital value or a multistate value.

Offline

If some of the objects are offline during a rename or delete, the system cannot update the references. In this case, the system informs you of the references that cannot be updated. You can still complete the procedure, but you have to keep track of the reference that are not updated. You can repair the references when the offline object is online again.

注释:

When changing the name of a folder or SmartStruxure server, you also have to reconfigure users and user groups path permissions to this SmartStruxure server or folder. 有关更多信息,请参阅 Path Permissions .

To rename a folder or object
  1. In WorkStation, in the System Tree pane, select the folder or object you want to rename.

  2. On the Edit menu, click Rename .

  3. In the Rename object dialog box, type the new name.

  4. Click OK .

  • Move, Copy, Paste, Rename, and Delete
  • Path Permissions
  • Updating References