You repair the License Administrator and the License Server installation if any problems are caused by the current installation.
To repair an installation, you must have access to the installation package that was used to install the product.
On the License Server, open the Service management console.
In Windows, open the Run dialog box and enter services.msc
In the Services console, right-click Building Operation x.x License Server .
Select Stop .
Double-click on the License Administrator installation file to start the installation wizard.
Click Yes to confirm that you want to run the License Administrator installation package.
Click Next .
Make sure that you agree with the End User License Agreement (EULA) and then click I Agree .
In the Program Files page, click Next .
In the Choose Components page, select the components you want to repair and then click Next .
In the Installation Type page, select Repair current version to repair the current License Administrator installation.
Click Next .
In the License Server page, in the License Server Address box, type @ and then type the address to the license server.
If the License Server uses a port other than the default port range 27000-27009, type the port number in front of @. For example, 567@localhost.
Use a semicolon to separate addresses to different License Servers.
Click Install .
In the Installation Complete page, click Next .
Click Show details to follow the progress of the installation.
Click Finish .