Use the Basic tab to configure and set up WebReports in WorkStation.
Property |
Description |
Web site URL |
Type the URL of the WebReports Web site. The URL includes the IP address of the Reports Server that is specified during the installation of WebReports. Type the complete URL, for example, http://10.159.17.246/SchneiderElectric/WebReports/Login.aspx |
Web service URL |
Type the URL of the WebReports Web service that requests and receives report names, and authenticates user logon information. The URL includes the IP address of the Reports Server that is specified during the installation of WebReports. Type the complete URL, for example, http://10.159.17.246/SchneiderElectric/WebReportsService |
Report source |
Verify that the default, WebReports , is selected. Do not change the default Report source . |
Default Report Folder Name |
Displays the name of the folder in the System Tree pane that is populated with factory supplied reports when WebReports is installed. You open the folder to select and view the factory supplied reports. You can also create and organize your own custom reports in the folder. Do not rename the folder. |