earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: WorkStation, WebReports
Funktionaliteter: Rapporter
Produktversion: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021-12-16

Report Output

arrow1_rotationExport Feature arrow1_rotationPrint Toolbar

When you have generated a report, you have a number of options for preserving the data contained in the report, for example you may want to print the report, or save it in a particular format such as a spreadsheet format.

You can perform the following operations after you generate a report:

  • Export the report to a PDF, Word, or Excel file.

  • Print the report.

  • Search for text in the report.

  • Navigate a multipage report.

Export Feature

Use the Export feature to save the report output as a PDF, Excel, or Word file. For example, suppose you generate an alarm report with a specific date range and want to save the report output. Using the Select a format option, you can select PDF, Excel, or Word and export the report. The report output is exported to a file in the format you selected.

 
action_zoom_plus_stroke Select a format and Export button
Figur: Select a format and Export button

Print Toolbar

Use the Print toolbar to print your report, search for text in the report, or navigate a multipage report.

 
action_zoom_plus_stroke Print toolbar
Figur: Print toolbar
  • WebReports Overview
  • Exporting a Report to a PDF, Excel, or Word File
  • Print Toolbar
  • Printing a Report