earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Report Types

arrow1_rotationPrompted Reports arrow1_rotationDashboard Reports

In WebReports, you can view and create two types of report: prompted reports, and dashboard reports.

Prompted Reports

A prompted report is a report that processes user-specified filtering criteria to generate the report output. With prompted reports, you enter and select filtering criteria for one or more input parameters, and then run the report. The generated report output provides information that is based on your filtering criteria.

有关更多信息,请参阅 提示报告 .

Dashboard Reports

A dashboard report is a report that processes fixed or predefined filtering criteria to generate report output.

Unlike prompted reports, dashboard reports process the report output based on the predefined filtering criteria and generate the report output when you select the report. You do not need to enter filtering criteria or click the Run button to generate the report.

有关更多信息,请参阅 仪表板报告 .

  • WebReports Overview
  • 提示报告
  • 仪表板报告