earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : License Administrator, License Server
Fonctionnalités : Gestion des licences
Version produit : 2.0, 2.1, 3.0, 3.1
14/05/2019

Resetting the License Server

You reset the License Server if it does not work correctly.

Déclaration

Loss of data

  • Return all the licenses to the License Activation Server before you reset the License Server. Resetting the License Server erases the licenses on the License Server.

Failure to follow these instructions can result in loss of data.

Afficher plus
action_close

If problems with the License Server or activated licenses occur, you may have to reset the License Server. All details about activated licenses on the License Server are compiled in files that start with "taclic" and have the .data extension. The file name string after "taclic" can differ. An example of the License Server file name is taclic_00249e00_tsf.data. The license details files are created the first time a license is activated on the License Server. By deleting the files you reset the License Server.

The license files are located in \ProgramData\FLEXnet.

Before deleting the License Server files, you have to return all activated network licenses to the License Activation Server.

Déclaration
  • If you delete the License Server files, all activated network licenses are lost.

To reset the License Server
  1. In License Administrator, click the Licenses view.

  2. In the Licenses view, select all the network licenses.

  3. On the Licenses toolbar, click the Remove/return license button

     
    action_zoom_plus_stroke
    .

  4. In the Licenses dialog box, click Yes .

  5. In the License Administrator , click Close .

  6. Close all EcoStruxure Building Operation programs that are running.

  7. Stop the License Server.

  8. In the License Server application folder, remove all .data files that start with taclic .

    The license files are located in \ProgramData\FLEXnet.

  9. Start the License Server.

  10. Reactivate the returned network licenses.

When you reactivate all returned network licenses, new License Server .data files are created together with the activation of the first license.

Déclaration

If the licenses cannot be returned, contact your local Customer Care Center to manually enter the license files into their server.

  • Stopping the License Server
  • License Administrator
  • Activating Network Licenses
  • Starting the License Server
  • License Server Reset
  • Unable to Check Out License
  • Problem with the Licenses on the License Server
  • EcoStruxure Building Operation Software Requirements