earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-L, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 1.9
2017/10/12

Restore Options Dialog Box

Use the Restore Options dialog box to select a backup set and the type of data that you want to restore. You can also import a backup set from a network storage location and restore the SmartStruxure server, or duplicate a SmartStruxure server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone Automation Server.

 
action_zoom_plus_stroke Restore Options dialog box
图: Restore Options dialog box

表格: Restore Options Dialog Box

Component

Description

Name

Displays the name of the backup set for the selected SmartStruxure server.

Created on

Displays the date the backup set was created.

Description

Displays a description of the backup set.

Configuration only

Select to restore only the configuration data and custom object type data. No historical data is restored.

All Data (Configuration and Historical)

Select to restore the historical data, configuration data, and custom object type data.

Import Backup Set

Click to import the backup set to a SmartStruxure server. In a multi-server configuration, you can import both Automation Server and Enterprise Server backup sets to the Enterprise Server.

Restore configuration with new IDs

Select to duplicate the configuration data from the imported backup set in the new standalone Automation Server. The communication settings from the backup set will not be duplicated.

有关更多信息,请参阅 Duplicate SmartStruxure Server Device from a Backup Set .

  • Backup Set Storage and Protection
  • Backup Set Import from WorkStation
  • Backup Options Dialog Box
  • Backup and Restore Manager on the Enterprise Server
  • Restore Incomplete Due to Network Connectivity Loss
  • No Restore Files Display After Backup
  • Renamed SmartStruxure Server Device Makes Backup Sets Unavailable
  • Duplicate SmartStruxure Server Device from a Backup Set
  • Backup Set Text is Red