Productos AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 3.2, 3.3
27/04/2023

Restoring the EcoStruxure BMS Server

You restore the EcoStruxure BMS server to revert back to a previous snapshot of the EcoStruxure BMS server data.

Mostrar más
action_close

Restore is the process of restoring data to an original or former state. Using Restore, you can revert to a previous snapshot of the EcoStruxure BMS server data despite any configuration changes made since the last backup. In the EcoStruxure BMS, Restore is a manual process designed to avoid the accidental overwriting of current EcoStruxure BMS server data.

Restored Data

Depending on what is contained in the backup file, you can restore different types of data.

  • Configuration only : the EcoStruxure Building Operation software restores the configuration database and custom object type data. Any existing historical data is lost when you select this option.

  • All data : the EcoStruxure Building Operation software restores the configuration, historical, and custom object types data.

Para obtener más información, consulte Restored Data .

SmartX Server Replacement Using Restore

Backup and Restore helps assure that SmartX server data can be restored to a replacement SmartX server in the event of detected failure, or to the same SmartX server in the event of data loss. As a precaution, you back up your SmartX servers regularly so that you can use the most current backup to restore the SmartX server data to a replacement SmartX server. You also configure the new SmartX server to match the name and the network settings of the replaced SmartX server so the system can identify this SmartX server when online.

Para obtener más información, consulte SmartX Server Replacement Using Restore .

Duplicate SmartX Server Using Restore

You can use the Restore function to re-use the configuration data from a backup set in a new standalone SmartX server. Rather than manually configuring your preferred SmartX server configuration, you can save time and configure the standalone SmartX server from a backup set.

The backup set used can originate from a SmartX server that is or has been part of a multi-server configuration.

Para obtener más información, consulte Duplicate SmartX Server from a Backup Set .

Aviso

If your system includes the Reports Server and the Enterprise Server or Enterprise Central, stop the Reporting Agent service on the Reports Server first to prevent report generation during a restore of the Enterprise Server or Enterprise Central. Para obtener más información, consulte Stopping the Reporting Agent Windows Service .

To restore the EcoStruxure BMS server
  1. Stop the Reporting Agent service on the Reports Server. Para obtener más información, consulte Stopping the Reporting Agent Windows Service .

  2. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server that you want to restore.

  3. On the Actions menu, click Restore .

    Aviso

    Take manual control of any output points that could potentially damage equipment before restoring the EcoStruxure BMS server. If you cannot disconnect the physical outputs, restore the EcoStruxure BMS server using a trusted restore file that will turn off/on the outputs predictably and safely.

  4. In the Restore Options dialog box, in the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the EcoStruxure BMS server.

  5. Select the type of data you want to restore:

    • Select Configuration only to restore only configuration and custom object types' data.

    • Select All data to restore the configuration, historical, and custom object types data.

  6. Click Restore .

  7. Click Yes .

  8. Click Close .

    If your system includes the Reports Server, the Reporting Agent Windows service restarts automatically.

  9. If you restore an Enterprise Central or an Enterprise Server that is not using the default ports, restart the server to restore the ports. Para obtener más información, consulte Restarting the Enterprise Server Windows Service .

  • Restore
  • Duplicate SmartX Server from a Backup Set
  • Restore Options Dialog Box
  • Restoring a SmartX Server from the Enterprise Server
  • Stopping the Reporting Agent Windows Service
  • Backup Set Text is Red
  • Restarting the Enterprise Server Windows Service