You restore the EcoStruxure BMS server to revert back to a previous snapshot of the EcoStruxure BMS server data.
If your system includes the Reports Server and the Enterprise Server or Enterprise Central, stop the Reporting Agent service on the Reports Server first to prevent report generation during a restore of the Enterprise Server or Enterprise Central. 有关更多信息,请参阅 Stopping the Reporting Agent Windows Service .
Stop the Reporting Agent service on the Reports Server. 有关更多信息,请参阅 Stopping the Reporting Agent Windows Service .
In WorkStation, in the System Tree pane, select the EcoStruxure BMS server that you want to restore.
On the Actions menu, click Restore .
Take manual control of any output points that could potentially damage equipment before restoring the EcoStruxure BMS server. If you cannot disconnect the physical outputs, restore the EcoStruxure BMS server using a trusted restore file that will turn off/on the outputs predictably and safely.
In the Restore Options dialog box, in the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the EcoStruxure BMS server.
Select the type of data you want to restore:
Select Configuration only to restore only configuration and custom object types' data.
Select All data to restore the configuration, historical, and custom object types data.
Click Restore .
Click Yes .
Click Close .
If your system includes the Reports Server, the Reporting Agent Windows service restarts automatically.
If you restore an Enterprise Central or an Enterprise Server that is not using the default ports, restart the server to restore the ports. 有关更多信息,请参阅 Restarting the Enterprise Server Windows Service .