earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 1.8, 1.9
2016/10/13

Restoring a SmartStruxure Server Device from the Enterprise Server

You log on to an Enterprise Server to restore a SmartStruxure server device.

显示更多
action_close

Restore is the process of restoring data to an original or former state. Using Restore, you can revert to a previous snapshot of the SmartStruxure server data despite any configuration changes made since the last backup. In Building Operation, Restore is a manual process designed to avoid the accidental overwriting of current SmartStruxure server data.

Restored Data

Depending on what is contained in the backup file, you can restore different types of data.

  • Configuration only : Building Operation restores the configuration database and custom object type data. Any existing historical data is lost when you select this option.

  • All data : Building Operation restores the configuration, historical, and custom object types data.

有关更多信息,请参阅 Restored Data .

SmartStruxure Server Device Replacement Using Restore

Backup and Restore assures that SmartStruxure server devices data can be restored to a replacement SmartStruxure server device in the event of hardware failure, or to the same SmartStruxure server device in the event of data loss. As a precaution, you back up your SmartStruxure server devices regularly so that you can use the most current backup to restore the SmartStruxure server devices data to a replacement SmartStruxure server device. You also configure the new SmartStruxure server device to match the name and the network settings of the replaced SmartStruxure server device so the system can identify this SmartStruxure server device when online.

有关更多信息,请参阅 SmartStruxure Server Device Replacement Using Restore .

Duplicate SmartStruxure Server Device Using Restore

You can use the Restore function to re-use the configuration data from a backup set in a new standalone SmartStruxure server device. Rather than manually configuring your preferred SmartStruxure server device configuration, you can save time and configure the standalone SmartStruxure server device from a backup set.

The backup set used can originate from a SmartStruxure server device that is or has been part of a multi-server configuration.

有关更多信息,请参阅 Duplicate SmartStruxure Server Device from a Backup Set .

To restore a SmartStruxure server device from the Enterprise Server
  1. In WorkStation, in the System Tree pane, select the SmartStruxure server device that you want to restore.

  2. On the Actions menu, click Restore .

    提示:

    Take manual control of any output points that could potentially damage equipment before restoring the SmartStruxure server device. If you cannot disconnect the physical outputs, restore the SmartStruxure server device using a trusted restore file that will turn off/on the outputs predictably and safely.

  3. In the Available restore points list, select a backup set in black text, which indicates that the backup set is compatible with the current version of the SmartStruxure server device.

     
    action_zoom_plus_stroke
  4. Select the type of data you want to restore:

    • Select Configuration only to back up only configuration and custom object types data.

    • Select All data to back up the configuration, historical, and custom object types data

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

    注释:

    After a restore, WorkStation may display several a SmartStruxure server device events in the Events pane that occurred while the restore was taking place. However, these events are not part of the restored log data.

  • Restore
  • Restoring the SmartStruxure Server
  • Restore Options Dialog Box
  • Backup Set Text is Red