Productos AS-C, AS-B, Enterprise Server, AS-P, Project Configuration Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.8
20/10/2016

Saving a Search

You save a search so you can reuse it later.

Mostrar más
action_close

Use Search in WorkStation to find and view objects in the database.

There are two different ways to search in WorkStation, Simple search and Advance search. An Advanced search can be done on, for example on conditions or objects types. An Advanced search can be saved for further use.

Search is case insensitive, which means that Search does not differ between upper case and lower case. A search on "Fan" results with hits on both "fan" and "Fan".

Simple Search

Use Simple search to search all objects names and properties names. The search results are displayed in a list.

Para obtener más información, consulte Simple Search .

Advanced Search

​Use the advanced search to filter and refine a search so you don’t get too many irrelevant results.

Para obtener más información, consulte Advanced Search .

Saved Search

Frequently used searches including the settings can be saved and reused.

A Saved search is displayed in the System Tree pane and the List View. To perform the search, open the Saved search from the System Tree pane or List View. The search results are displayed in the work area (with collapsed Search criteria area).

A Saved search can be changed, renamed, and deleted.

Aviso
  • When you save a search, only the setting for the search is saved. The search result is never saved.  

To save a search
  1. In WorkStation, on the Search toolbar, click the Save search criteria button

     
    action_zoom_plus_stroke
    .

  2. Enter the location where you want to save the search.

  3. In the Name box, type a name.

  4. Click Save .

  • Search Overview
  • Search View Toolbar