earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface utilisateur

Interface utilisateur


Produits : AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Calendriers
Version produit : 2023
21/05/2024

Boîte de dialogue Propriétés d'événement horaire – Vue d'exception calculée

Utilisez la vue Exception calculée dans la fenêtre de dialogue Propriétés des événements horaires pour programmer des exceptions récurrentes.

 
action_zoom_plus_stroke Boîte de dialogue Propriétés d'événement horaire – Vue d'exception calculée
Figure : Boîte de dialogue Propriétés d'événement horaire – Vue d'exception calculée

Table : Boîte de dialogue Propriétés d'événement horaire – Vue d'exception calculée

Composant

Description

Type d'événement

Cliquez sur Exception pour afficher les types d'exception.

Type d'exception

Sélectionnez Calculé pour le type d'exception à appliquer au programme horaire.

 
action_zoom_plus_stroke

Click to add a line to the Times and values box.

 
action_zoom_plus_stroke

Click to delete an entry from the Times and values box.

Toute la journée

Select to create an all day event.

Nom

Type a name for the event.

Priorité

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Année

Affiche l'année courante , qui est la valeur par défaut de la vue d'exception calculée.

Mois

Select a month for the exception event or Odd month , Even month , Any month .

Semaine du mois

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. The second week is then considered day of month eight through fourteen and so on. Since the dates do not necessarily correspond to the first row of the calendar, they may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Semaine du mois

Select a week of the month for the exception event or First week , Second week , Third week , Fourth week , Last week , Any week .

  • First week – the first through the seventh day of the month. Be aware that it does not necessarily correspond to the first row of the calendar since it may include dates from both the first and second row of the calendar.

  • Fifth week – days 29 through 31 if they exist. It is always less than seven days and is non-existent in February except in a leap year.

  • Last week – the last seven days of the month. It differs from the Fifth wee k .

Jour de la semaine

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Événements exceptionnels dans WorkStation