earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Programaciones
Versión del producto: 2024, 7.0
02/12/2024

Schedule Event Properties Dialog Box – Single Date Exception View

Use the Single Date Exception view in the Schedule Event Properties dialog box to schedule a single date exception.

 
action_zoom_plus_stroke Schedule Event Properties dialog box - Single date exception view
Figura: Schedule Event Properties dialog box - Single date exception view

Tabla: Schedule Event Properties Dialog Box – Single Date Exception View

Component

Description

Event type

Click Exception to display the exception types.

Exception type

Select Single date for the exception type to apply to the schedule.

 
action_zoom_plus_stroke

Click to add a line to the Times and values box.

 
action_zoom_plus_stroke

Click to delete an entry from the Times and values box.

All Day

Select to create an all day event.

Name

Type a name for the exception event.

Priority

Select a priority number between 1 (highest priority) and 16 (lowest priority).

Year

Select a year. You can use Any year as a valid entry.

Month

Select a month for the exception event or Odd month , Even month , Any month .

Day of month

Select a value for the day of the month. You can use Any Day , Last day , Odd days or Even days as valid entries.

Day of week

Select a day of the week. Setting the value to Any Day ensures consistency with the rest of the date specification, this is the recommended setting.

  • Exception Events in WorkStation