Produkty: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funkcje: Harmonogramy
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Schedule Event Properties Dialog Box – Weekly View

Use the Weekly View in the Schedule Event Properties dialog box in the Basic Schedule Editor to create a new weekly event for an existing schedule.

 
action_zoom_plus_stroke Schedule Event Properties dialog box - weekly view
Rysunek: Schedule Event Properties dialog box - weekly view

Tabela: Schedule Event Properties Dialog Box – Weekly View

Component

Description

Event type

Click Weekly to select a weekly event type.

Days of week

Select the days of the week that apply to this schedule.

 
action_zoom_plus_stroke

Click to add a line to the Times and values box.

 
action_zoom_plus_stroke

Click to delete an entry from the Times and values box.

All day

Select to create an all day event.

  • Weekly Events in WorkStation