earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, WorkStation, Project Configuration Tool
Funcionalidades: Agendas
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Schedule Event Properties Dialog Box – Weekly View

Use the Weekly View in the Schedule Event Properties dialog box in the Basic Schedule Editor to create a new weekly event for an existing schedule.

 
action_zoom_plus_stroke Schedule Event Properties dialog box - weekly view
Imagem: Schedule Event Properties dialog box - weekly view

Tabela: Schedule Event Properties Dialog Box – Weekly View

Component

Description

Event type

Click Weekly to select a weekly event type.

Days of week

Select the days of the week that apply to this schedule.

 
action_zoom_plus_stroke

Click to add a line to the Times and values box.

 
action_zoom_plus_stroke

Click to delete an entry from the Times and values box.

All day

Select to create an all day event.

  • Weekly Events in WorkStation