A schedule has two types of events: weekly events and exception events. Weekly events occur every week at specified times. Exception events occur when the schedule deviates from the weekly schedule, such as during holidays. Exception events override the weekly events when there is an overlap.
对于除 Xenta 时间表之外的每个时间表,您可以设置默认值。默认值会在例外事件和每周事件完成或放弃控制后生效。例如,风机的每周事件在 17:00 结束。在整个事件中,风机以值 3(高)运行。每周事件后没有时间表事件。因为您已指定 0 作为默认值,风机会调整到默认值并转到 0(关闭)。值始终保持为 0,直到下一个时间表事件。
事件以下列顺序发生:
例外事件
每周事件
默认值
Xenta 时间表没有任何默认值。
示例:
风机的每周事件设为 08:00 - 17:00。例外事件设为特定日期的 17:00 - 20:00。例外事件会覆盖每周事件,因此风机只在特定日期的 17:00 到 20:00 运行。
Xenta 时间表事件以下列顺序发生:
例外事件
每周事件
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
有关更多信息,请参阅 WorkStation 中的每周事件 .
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
有关更多信息,请参阅 Webstation 中的每周事件 .
An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.
有关更多信息,请参阅 WorkStation 中的例外事件 .
An exception event occurs instead of the scheduled weekly events for a single date, date range, calculated date, or calendar reference.
有关更多信息,请参阅 Webstation 中的例外事件 .
Priority is a number that corresponds to a preassigned level of importance. When used in schedules, priority numbers range from one to sixteen. One is the most important or highest priority and sixteen is the lowest priority.
有关更多信息,请参阅 Priorities .
When you create a schedule, the time zone of the EcoStruxure BMS server that contains the schedule determines the execution of the events. If the schedule is copied to an EcoStruxure BMS server in a different time zone, the specified dates and times relate to the new time zone.
有关更多信息,请参阅 Time Zones .