Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The Schedule Report Activity report provides information about WebReports Schedules. You can use the report to identify whether a Reports schedule ran successfully, the number of times the schedule ran, and the average amount of time, in seconds, that the schedule ran.
|
Input Parameters |
Description |
|
Start report date/time |
Specifies the start date and time of the Reports schedule operation. |
|
End report date/time |
Specifies the end date and time of the Reports schedule operation. Information about all Reports schedules that failed or succeeded between your start and end dates and times displays in the report. |
|
Date range filter |
Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent. For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days. Select Fixed date if you entered a Start report date/time and an End report date/time .
|
|
Status |
Specifies the status types, Success , Fail , or Error that can be displayed in the report. |
|
Event type |
Specifies the event types, Information , or Error , that can be displayed in the report. |
|
Minimum generation time (s) |
Specifies the amount of time, in seconds, required to run the Reports schedule. For example, if you enter 5 seconds, the report displays information about all Report schedules that required 5 seconds or more to run. If you enter 0, the report displays information about all Report schedules that ran regardless of the amount of time required to run. |