earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos WebReports
Funcionalidades: Informes
Versión del producto: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
16/12/2021

Schedule Report Activity Report

The Schedule Report Activity report provides information about WebReports Schedules. You can use the report to identify whether a Reports schedule ran successfully, the number of times the schedule ran, and the average amount of time, in seconds, that the schedule ran.

Tabla: Schedule Report Activity Input Parameters

Input Parameters

Description

Start report date/time

Specifies the start date and time of the Reports schedule operation.

End report date/time

Specifies the end date and time of the Reports schedule operation. Information about all Reports schedules that failed or succeeded between your start and end dates and times displays in the report.

Date range filter

Specifies the date range of an operation, such as an alarm trigger, the running of a report schedule, or a read by the Reporting Agent.

For example, if you select Last 7 days for an alarm report, the report displays information about all alarms that were triggered during the last 7 days. If you select Last 7 days for the Report schedule report, the report displays information about all Report schedules that were run during the last 7 days. If you select Last 7 days for the Reporting Agent report, the report displays information about all Reporting Agent reads that occurred during the last 7 days.

Select Fixed date if you entered a Start report date/time and an End report date/time .

Status

Specifies the status types, Success , Fail , or Error that can be displayed in the report.

Event type

Specifies the event types, Information , or Error , that can be displayed in the report.

Minimum generation time (s)

Specifies the amount of time, in seconds, required to run the Reports schedule. For example, if you enter 5 seconds, the report displays information about all Report schedules that required 5 seconds or more to run. If you enter 0, the report displays information about all Report schedules that ran regardless of the amount of time required to run.

  • Factory Supplied Reports
  • Production Reports
  • WebReports Submit Form Page