You can create three types of schedules: Digital, Multistate, or Analog. You create a digital schedule if the schedule needs to control a device with two output states, such as On or Off. You create a multistate schedule if the schedule needs to control a device that has output states based on multiple states, such as low, medium, or high. You create an analog schedule if the schedule controls a device that gauges the output in real numbers.
You create schedules using WorkStation.
An analog schedule controls a device that gauges the output in real numbers. The real numbers include positive or negative numbers, fractions, and decimal values.
Więcej informacji zawiera Analog Schedules .
A digital schedule controls a device that has an on output state and an off output state.
Więcej informacji zawiera Digital Schedules .
A multistate schedule controls a device that has output states based on integers or positive whole numbers including zero.
Więcej informacji zawiera Multistate Schedules .