earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concepto

Concepto


Productos Enterprise Server, Project Configuration Tool
Funcionalidades: Funcionalidad básica
Versión del producto: 1.9
14/12/2016

Archiving SmartStruxure Server Compatibility

You can configure archiving on an Enterprise Server.

The following table lists the SmartStruxure servers that support archiving capabilities.

Tabla: Archiving and SmartStruxure Server Compatibility Matrix

Server

Runtime Archiving?

Description

Enterprise Server

Yes

You can configure and manage archiving on an Enterprise Server.

SmartStruxure server device

No

You cannot configure or initiate archiving on a SmartStruxure server device. The system only archives data from trend logs or extended trend logs on SmartStruxure server devices that are monitored by extended trend logs on the Enterprise Server.

  • Archiving Overview
  • Enabling the Archiving Function and Defining the Archive Folder