earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Produits : Enterprise Central, Enterprise Server, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 3.3, 2022, 2023, 2024
23/07/2021

Archiving EcoStruxure BMS Server Compatibility

You can configure archiving on an Enterprise Server or an Enterprise Central.

The following table lists the EcoStruxure BMS servers that support archiving capabilities.

Table : Archiving and EcoStruxure BMS Server Compatibility Matrix

Server

Runtime Archiving?

Description

Enterprise Server

Yes

You can configure and manage archiving on an Enterprise Server.

Enterprise Central

Yes

You can configure and manage archiving on an Enterprise Central.

automation server

No

You cannot configure or initiate archiving on an automation server. The system only archives data from trend logs or extended trend logs on automation servers that are monitored by extended trend logs on the Enterprise Server.

  • Archiving Overview
  • Enabling the Archiving Function and Defining the Archive Folder