earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2
2018/6/25

Archiving EcoStruxure BMS Server Compatibility

You can configure archiving on an Enterprise Server or an Enterprise Central.

The following table lists the EcoStruxure BMS servers that support archiving capabilities.

表格: Archiving and EcoStruxure BMS Server Compatibility Matrix

Server

Runtime Archiving?

Description

Enterprise Server

Yes

You can configure and manage archiving on an Enterprise Server.

Enterprise Central

Yes

You can configure and manage archiving on an Enterprise Central.

SmartX server

No

You cannot configure or initiate archiving on a SmartX server. The system only archives data from trend logs or extended trend logs on SmartX servers that are monitored by extended trend logs on the Enterprise Server.

  • Archiving Overview
  • Enabling the Archiving Function and Defining the Archive Folder