earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: WebStation
功能: 时间表
产品版本: 1.8
2016/6/10

Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation

You edit a weekly event to change the time range, start and stop time, or weekdays of the weekly event.

显示更多
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. You can assign and unassign lead Xenta central schedules. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

有关更多信息,请参阅 时间表运作方式 .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

有关更多信息,请参阅 Xenta Central Schedules .

重要:

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

To edit or delete a weekly event in a Xenta schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule containing the weekly event you want to edit.

  2. In the Xenta Schedule editor, click

     
    action_zoom_plus_stroke
    .

  3. In the Span column, select Interval or On all day .

     
    action_zoom_plus_stroke
  4. If you select Interval , select the start time and the end time.

  5. Select the weekdays the weekly event is to be in service.

  6. Click Save .

To delete a weekly event, click the trash can.

  • Xenta Schedules in WebStation
  • Adding a Weekly Event to a Xenta Schedule in WebStation