Use Search to find and view objects in the EcoStruxure Building Operation database.
There are two different ways to search in WebStation:
The Search function searches for all object names and property names in the system.
A saved search is a predefined search that searches specific criteria in a specific part of the system. Saved searches are created in WorkStation and the search criteria cannot be changed in WebStation.
Search is case insensitive, which means that Search does not distinguish between uppercase and lowercase letters. A search for "Fan" results with hits for both "fan" and "Fan".
Use wildcards to substitute characters or combinations of characters in a search.
Search supports two main wildcards:
Asterisk (*) represents any combination of characters including white space.
Question mark (?) represents any single character.
For example, you want to find all objects and properties containing the word “Temperature”. You start the search with an asterisk so that the search includes all hits on objects like “Outside Air Temperature” where the asterisk represents the words before "Temperature", in this case “Outside Air”. You also have to end the search text with an asterisk to include objects like “Temperature Alarm” where the asterisk represents the word after "Temperature", in this case “Alarm”.
When you perform a search, you cannot leave the Search box empty. To perform a search, you have to enter something in the Search box.