Use Search in WorkStation to find and view objects in the database.
There are two different ways to search in WorkStation, Simple search and Advance search. An Advanced search can be done on, for example on conditions or objects types. An Advanced search can be saved for further use.
Search is case insensitive, which means that Search does not differ between upper case and lower case. A search on "Fan" results with hits on both "fan" and "Fan".
Use Simple search to search all objects names and properties names. The search results are displayed in a list.
For more information, see Simple Search .
Use the advanced search to filter and refine a search so you don’t get too many irrelevant results.
For more information, see Advanced Search .
Frequently used searches including the settings can be saved and reused.
A Saved search is displayed in the System Tree pane and the List View. To perform the search, open the Saved search from the System Tree pane or List View. The search results are displayed in the work area (with collapsed Search criteria area).
A Saved search can be changed, renamed, and deleted.
When you save a search, only the setting for the search is saved. The search result is never saved.