earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.9
2/22/2017

Searching for Objects Using Simple Search

You use Simple search to search for an object by its name.

Show More
action_close

Use Search in WorkStation to find and view objects in the database.

There are two different ways to search in WorkStation, Simple search and Advance search. An Advanced search can be done on, for example on conditions or objects types. An Advanced search can be saved for further use.

Search is case insensitive, which means that Search does not differ between upper case and lower case. A search on "Fan" results with hits on both "fan" and "Fan".

Simple Search

Use Simple search to search all objects names and properties names. The search results are displayed in a list.

For more information, see Simple Search .

Advanced Search

​Use the advanced search to filter and refine a search so you don’t get too many irrelevant results.

For more information, see Advanced Search .

Saved Search

Frequently used searches including the settings can be saved and reused.

A Saved search is displayed in the System Tree pane and the List View. To perform the search, open the Saved search from the System Tree pane or List View. The search results are displayed in the work area (with collapsed Search criteria area).

A Saved search can be changed, renamed, and deleted.

Note:
  • When you save a search, only the setting for the search is saved. The search result is never saved.  

Relative or Locked Search Path

If you want to reuse your saved Search object in similar folder structures, you can enter a relative search path in your saved Search object. You can reuse a saved Search object by using export and import or copy and paste special.

If you have configured your Search object with a relative reference, the search result is performed on a path relative to the location of the saved Search object.

If you have configured your Search object with a locked reference, the search is performed on the specific folder or container object even if the folder or container object is renamed or moved. By default, search paths are locked.

Table: Locked and Unlocked References

Path reference syntax

Description

~

Locked reference

Searches in the configured folder or container object

../..

Relative reference

Searches in a path relative to where the Search object is saved. For example, entering '../../' in the folder path means that the search is performed two levels up from where the Search object is saved.

To perform a search using simple search
  1. In WorkStation, in the Search box, enter the text you want to search for.

  2. Click the Search button

     
    action_zoom_plus_stroke
    .

The search result is presented in the Search view list.

  • Simple Search
  • Search Toolbar