earth_america
user_standard Accedi
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaccia dell'utente

Interfaccia dell'utente


Prodotti: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funzionalità: Funzionalità di base
Versione del prodotto: 3.2, 3.3, 2022
15/10/2020

Select Conditions Dialog Box

Use the Select Conditions dialog box to enter property criteria for the object types that are included in the search.

 
action_zoom_plus_stroke Select conditions dialog box with the common properties for all object types.
Figura: Select conditions dialog box with the common properties for all object types.

Tabella: Select Conditions Dialog Box

Button

Description

 
action_zoom_plus_stroke

Click to add a condition.

 
action_zoom_plus_stroke

Click to remove a condition.

  • Search Overview
  • Search View Toolbar
  • Select Folder Dialog Box
  • Select Types Dialog Box