earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2024, 7.0
2024/12/2

Series Tab Context Menu

Use the series tab context menu to change the presentation of series, show or hide events, markers, and series, bring to front and remove series, as well as open the trend chart settings dialog box.

The series tabs are located at the bottom leftmost if there are series attached to the left y-axis, and at the bottom rightmost if there are series attached to the right y-axis.

 
action_zoom_plus_stroke Series tab context menu
图: Series tab context menu

表格: Series Tab Context Menu

Component

Description

Line

Select to display the series as a line.

Discrete line

Select to display the series as a discrete line.

Digital

Select to display the series as a digital line.

Bars

Select to display the series as bars.

Events

Select to present the series with event symbols.

Visible

Select to hide or display the series in the trend chart.

Markers

Select to display a marker for each record. Markers can only be shown for lines and discrete lines, not for digital and bars.

Bring to front

Click to display the series in front of the others.

Remove series

Click to remove series from the trend chart.

Open trend chart settings

Click to open the property dialog box for the trend chart and its series.

  • Trend Charts
  • Trend Chart View
  • Trend Chart Event Icons
  • Trend Chart Does Not Show Trend Log Series