earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Shortcut Functionality

When you click on a shortcut to an object in the System Tree pane, the appropriate view for the target object (such as a graphic or a properties dialog box) is displayed. If you view the Properties of a selected shortcut, the properties shown are always those of the target object. However, if you view the Shortcut Properties of a selected shortcut, the properties shown are those of the shortcut.

When you select a shortcut, the address bar shows the address of the shortcut and the icon of the shortcut becomes highlighted. Also, the name displayed on the window tab is that of the shortcut.

You can reference a shortcut as if it were the target object. For example, if you drag a shortcut to the Watch pane, the target object is added to the Watch pane as if it had been dropped there instead. This functionality also applies to other situations such as logging and alarms.

Shortcut object commands that create new objects referencing the target (such as a new alarm or trend log) create the new objects at the parent folder of the shortcut (not the parent folder of the target).

Shortcuts are followed whenever a selection action is performed, except in the following circumstances:

  • When the target value is Null

  • When exporting objects (the shortcut is exported, not the target)

  • When displaying the shortcut object properties using the Shortcut Properties command in the context menu

  • Function Overview
  • Shortcuts Overview