earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2024, 7.0
12/2/2024

Shortcut Properties – Basic Tab

Use the Basic tab to view shortcut properties or to change the path to the target object in the System Tree pane.

 
action_zoom_plus_stroke Basic tab
Figure: Basic tab

Table: Basic Tab

Component

Description

Target

Enter the path of the target EcoStruxure BMS server, folder, or object.

  • General Information Properties – Basic Tab
  • References Tab
  • Shortcut Creation
  • Viewing Shortcut Properties