Funktionaliteter: Grundläggande funktionalitet
Produktversion: 2024, 7.0
2024-12-02

Object Tab Display

You can make WorkStation open the same tab each time you navigate between objects.

For example, you want to check all alarm messages in your alarms. The default behavior in WorkStation is that the Basic Settings tab is displayed whenever you click on an alarm object. You can have the system display the Presentation tab of the Alarm object every time you click on an Alarm object.    

  • Options Dialog Box
  • Showing the Same Tab While Navigating Between Objects