You show hidden alarms when you want them to be displayed in the Alarms pane or Alarm View.
In WorkStation, in the Alarms pane or Alarm View, on the Alarm toolbar, click the Show hidden alarms button
In the Alarms pane, right-click the alarm and then click Show alarm .
The alarm is displayed in the Alarms pane or Alarm View when it is in an alarm state.