Funkcje: Podstawowa funkcjonalność
Wersja produktu: 3.2, 3.3, 2022
2020-10-15

Signal Generator Properties - Basic Tab

Use the Signal Generator properties Basic tab to configure a sinus, square, or saw tooth signal used for tests.

 
action_zoom_plus_stroke Signal generator dialog box 
Rysunek: Signal generator dialog box 

Component

Description

Value

Select the signal value and whether to force or unforce the value.

Signal type

Select the signal type, sinus, square, saw tooth, setpoint, alarm, or event.

Cycle (s)

Select the cycle in seconds.

Amplitude

Select the amplitude.

  • Creating a Utility Object
  • General Information Properties – Basic Tab
  • References Tab
  • Simple Math Operator Properties - Basic Tab
  • Create Object Dialog – Naming the Object Page
  • Forced Values