earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidade básica
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Signal Generator Properties - Basic Tab

Use the Signal Generator properties Basic tab to configure a sinus, square, or saw tooth signal used for tests.

 
action_zoom_plus_stroke Signal generator dialog box 
Imagem: Signal generator dialog box 

Component

Description

Value

Select the signal value and whether to force or unforce the value.

Signal type

Select the signal type, sinus, square, saw tooth, setpoint, alarm, or event.

Cycle (s)

Select the cycle in seconds.

Amplitude

Select the amplitude.

  • Creating a Utility Object
  • General Information Properties – Basic Tab
  • References Tab
  • Simple Math Operator Properties - Basic Tab
  • Create Object Dialog – Naming the Object Page
  • Valores forçados