earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2023
2022/12/17

Signal Generator Properties - Basic Tab

Use the Signal Generator properties Basic tab to configure a sinus, square, or saw tooth signal used for tests.

 
action_zoom_plus_stroke Signal generator dialog box 
图: Signal generator dialog box 

Component

Description

Value

Select the signal value and whether to force or unforce the value.

Signal type

Select the signal type, sinus, square, saw tooth, setpoint, alarm, or event.

Cycle (s)

Select the cycle in seconds.

Amplitude

Select the amplitude.

  • Creating a Utility Object
  • General Information Properties – Basic Tab
  • References Tab
  • Simple Math Operator Properties - Basic Tab
  • Create Object Dialog – Naming the Object Page
  • 强制值的概念