earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 基本功能
产品版本: 2024, 7.0
2024/12/2

Simple Math Operator Properties - Basic Tab

Configure the Simple Math Operator properties Basic tab to add, subtract, multiply, or divide one value from another when you perform tests.

 
action_zoom_plus_stroke Simple math operator
图: Simple math operator

Component

Description

Operator

Select the operator, add, subtract, multiply, or divide.

In1

Input value 1.

In2

Input value 2.

Value

Displays the calculated value.

  • Creating a Utility Object
  • General Information Properties – Basic Tab
  • References Tab
  • Signal Generator Properties - Basic Tab
  • Create Object Dialog – Naming the Object Page
  • Forced Values