Produkty: Enterprise Central, Enterprise Server, Software Administrator
Funkcje: Inżynieria
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-10-25

Software Administrator – Enterprise Server View

Use the Enterprise Server view ​to start and stop the Enterprise Server service and configure the ports of the Enterprise Server.

 
action_zoom_plus_stroke Enterprise Server view
Rysunek: Enterprise Server view

Tabela: Enterprise Server View

Component

Description

Status

Displays the current status of the Enterprise Server Windows service.

Start Service

Click to start the Enterprise Server.

Stop Service

Click to stop the Enterprise Server.

HTTP Port

Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol.

HTTPS Port

Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol Secure.

TCP Port

Type the port number that the Enterprise Server listens to when communicating through the Transmitting Control Protocol.

System

Displays the system log.

Path

Displays the path to the folder where the Enterprise Server database and other objects created by the Enterprise Server or users are stored.

 
action_zoom_plus_stroke

A warning indicates that you entered a conflicting port number or that the service is stopping.

  • Starting the Enterprise Server or Enterprise Central Windows Service
  • Stopping the Enterprise Server Windows Service
  • Restarting the Enterprise Server Windows Service
  • Software Administrator
  • ​Configuring Server Port Settings