Software permissions are used to manage privileges that user account groups and user accounts own to objects in Building Operation software. In the EcoStruxure Building Operation software, you can assign two types of software permissions to user account groups and user accounts: path permissions and command permissions. You can also assign extended permissions to all the instances of folder structure or of a custom type.
Path permissions grant a specific set of permissions to a user account or a user account group to all the folders and objects defined in a path in the EcoStruxure Building Operations software.
For more information, see Path Permissions .
Command permissions grant a specific set of permissions to a user account or a user account group to commands in the EcoStruxure Building Operation database. You use command permissions to configure exceptions from path permissions.
For more information, see Command Permissions .
Extended Permissions are used to manage privileges of a user account group or a user account with respect to the instances of a folder structure or to the instances of custom type.
There are two types of extended software permissions:
Relative path permissions. For more information, see Relative Path Permissions .
Type permissions. For more information, see Type Permissions .
Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.
For more information, see Relative Path Permissions .
Extended permissions for a type grant a specific set of permissions to a user accounts group or to a user account to all instances of this type. There are two types of type permissions. Custom type permissions grant permissions for types created by the users. In-build type permissions grant permissions for types provided by default with the system.
For more information, see Type Permissions .
Software permissions can be combined between them.
For more information, see Software Permissions Management .