earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 用户管理
产品版本: 2024
2024/12/2

Software Permissions

arrow1_rotationPath Permissions arrow1_rotationCommand Permissions arrow1_rotationExtended Software Permissions arrow1_rotationRelative Path Permissions arrow1_rotationType Permissions arrow1_rotationSoftware Permissions Management

Software permissions are used to manage privileges that user account groups and user accounts own to objects in Building Operation software. In the EcoStruxure Building Operation software, you can assign two types of software permissions to user account groups and user accounts: path permissions and command permissions. You can also assign extended permissions to all the instances of folder structure or of a custom type.

Path Permissions

​Path permissions are used to give a user account group or a user account access to the objects defined in the path. Path permissions can also be set on specific properties. The permissions configured on a path apply to all path sub-levels unless you configure new permissions for the path sub-level.

有关更多信息,请参阅 Path Permissions .

Command Permissions

Command permissions grant a specific set of permissions to a user account or a user account group to commands in the EcoStruxure Building Operation database. You use command permissions to configure exceptions from path permissions.

有关更多信息,请参阅 Command Permissions .

Extended Software Permissions

Extended Permissions are used to manage privileges of a user account group or a user account with respect to the instances of a folder structure or to the instances of custom type.

There are two types of extended software permissions:

Relative Path Permissions

Relative path permissions for a folder structure grant a specific set of permissions to a user account group or to a user account to all the folders accessible in a predefined path and its folder structure. Relative path permissions enable a user accounts group or a user account to reuse a specific path permission.

有关更多信息,请参阅 Relative Path Permissions .

Type Permissions

Extended permissions for a type enable you to provide additional permissions for a particular user or groups of users by granting a specific set of permissions to a user accounts group or to a user account to all instances of this type. The purpose of extended type permissions is to increase the permissions for a specific type. There are two types of type permissions. Custom type permissions grant permissions for types created by the users. In-build type permissions grant permissions for types provided by default with the system.

有关更多信息,请参阅 Type Permissions .

Software Permissions Management

Software permissions can be combined between them.

有关更多信息,请参阅 Software Permissions Management .

  • User Account Management Overview
  • Path Permissions
  • Command Permissions
  • Extended Software Permissions
  • Relative Path Permissions
  • Type Permissions
  • Software Permissions Management