earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AS-L, AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 趋势
产品版本: 2.0, 2.1, 3.0, 3.1
2018/5/18

Trend Log Activation

arrow1_rotationActivation Variable arrow1_rotationStart at activation time

​The interval trend log and change of value trend log start recording values when the configured activation conditions are met. If an activation variable is used, both the activation variable and the activation time have to be true for the trend log to start recording.

On all trend logs, you can stop recording values by disabling the trend log. To resume recording, you enable the trend log. 有关更多信息,请参阅 Disabling a Trend Log .

Activation Variable

You configure an activation variable to have the trend log start recording values when a connected variable goes on. This variable can be a scheduled variable or a variable from a switch.

You can also have the trend log stop recording when the variable, such as a fan, goes off. For example, you can use this feature to log the effective time a fan is on.

 
action_zoom_plus_stroke Activation variable that follows the activation time
图: Activation variable that follows the activation time

Start at activation time

You configure an activation time to have the trend log start recording values at a specified time.

For Interval Trend Logs, the logging interval is aligned with the activation time. 有关更多信息,请参阅 间隔趋势日志 .

 
action_zoom_plus_stroke Trend log that starts recording at activation time
图: Trend log that starts recording at activation time
  • Trend Log Functions
  • Trends Overview
  • 间隔趋势日志
  • Interval Trend Log Properties – Basic Tab
  • Change of Value Trend Log Properties – Basic Tab
  • Variable Triggered Trend Log Properties – Basic Tab
  • Actions Menu – Activation Submenu
  • 创建间隔趋势日志
  • 编辑间隔趋势日志的间隔
  • Configuring a Change of Value Trend Log
  • Disabling a Trend Log
  • Enabling a Trend Log